8/5/2015 1:45 PM | |
Posts: 122 Rating:
|
Hello! I meet some problems with profibus and need help from experts. Is used PLC S7-400 with CP 443-5 Ext as master profibus. This network contains 97 slaves. Most of all are ET200B, ET200M and PP17. Baud rate is 187.5Kb/s. Total length is around 1500 meters. 11 Reapeters are used in this network (successive maximum 6). For diagnose is used FrofiTrace tool. All segments bettwen reapeters was tested and signal is strong, no reflection, no short circuit and wire break. But in some times profibus get down, not all but only several stations, different times - different stations. In attached screens you can see print screen of diagnostic diagram. On procentec site I found this FAQ:
In HW config these options are not aviable to change. Please give some advises how change these values. And what to do more to get a stable comunication. Attachmentbus_picts.rar (104 Downloads) |
8/5/2015 2:54 PM | |
Posts: 122 Rating:
|
Thank you. I already set these values of net lenght and reapeaters count. But is it possibile to change: Retries limit, Tqui, MinTSDR |
8/5/2015 3:08 PM | |
Joined: 12/16/2012 Last visit: 3/16/2025 Posts: 655 Rating:
|
Hi! In the Properties window choose "User-defined" instead of DP |
This contribution was helpful to
1 thankful Users |
8/5/2015 3:59 PM | |
Posts: 122 Rating:
|
Thank you Kahl |
This contribution was helpful to
1 thankful Users |
Follow us on