11/10/2009 5:54 AM | |
Joined: 1/16/2008 Last visit: 3/14/2025 Posts: 17 Rating:
|
Dear Friends, We are configuredthe two 315-2 PN/DP for PROFINET communication for that we are used the O C Wizard Entry ID 25209116; also we referred the sample program from entry ID 25209116 (Having problem in CPU 319-2 PN/DP ---data block DB10). As per sample program we also used FB65, FB64, FB63, and FB66 for communication & data send / receive in between two CPU 315-2PN/DP But when we given request to TCON block FB65 for both the CPU it always gives Status 7000 or 7002 means request is in process or request not available. Pl find here with attached program for reference. Thanks in advance. Regards, Sagar Gilankar AttachmentProfinet.zip (222 Downloads) |
11/19/2009 4:20 PM | |
Posts: 5822 Rating:
|
Dear Sagar, I admit, I have no idea what is going wrong with your system. I hope you really have a CPU with Version 2.5 and higher as you configured it. To try I added two DBs to each of your Systems. One with ID 1 created by the Open Communication Wizard (DB2)... up to date, and a second one (DB3) with a Connection for both stations in one Open Communication Wizard cycle. Hopefully this will fix your issue. Best regards J_Bell AttachmentProfinet2.zip (283 Downloads) |
Last edited by: J_Bell at: 11/19/2009 4:22 PM |
|
Follow us on