3/16/2016 1:26 AM | |
Joined: 11/13/2015 Last visit: 7/22/2022 Posts: 8 Rating:
|
Hello everyone, I have the same problem. I have in my TIA PORTAL V13 project two CPUs (S7315 2PN/DP and S7-1214C DC/DC/Rly) communicating over Profinet. I created a S7_Connection between the controllers, the program create automatically two connections (1o connection S7-315 2PN/DP x S7-1214C / 2o connection S7-1214C x S7-315 2PN/DP) named "S7_Connection_1" by default and assign automatically ID 10 to S7-315 2PN/DP and ID 100 to S7-1214C. In the S7-315 2PN/DP configuration of GET block I insert 0.5hz bit for REQ and in configuration I select S7-1214C CPU as target and select "S7_Connection_1". S7-315 2PN/DP will be the server and insert blocks PUT and GET to read and write data to S7-1214C but without success. Can anyone help me? ------------------------------------------------------------------------------------------ |
Last edited by: HTrebilcock at: 3/16/2016 2:41:28 AMLast edited by: Min_Moderator at: 3/16/2016 12:38:04 PMNew subject after splitting |
|
Follow us on