5/17/2017 11:41 AM | |
Posts: 27 Rating: (0) |
dear sir if u have command address manual of g120 ( cu240e-2). pls send me thanks |
5/17/2017 11:50 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hi, install Startdrive to add the G120 to the HWCatalog of tia. Then create a S7-1200 and from the catalog select the G120 you need. Now you can configure a data transfer telegram on the G120 in Device properties . You can create a speedaxis on the S7-1200 and connect it woth the G120, now you can use the MotionControl commands in your block on S7-1200. What you mean with command adress manual? Application Example: https://support.industry.siemens.com/cs/ww/en/view/70155469 Regards Christoph |
5/17/2017 12:34 PM | |
Posts: 27 Rating: (0) |
|
5/17/2017 12:37 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
https://support.industry.siemens.com/cs/ww/de/view/109741912 |
5/17/2017 12:44 PM | |
Posts: 27 Rating: (0) |
dear sir this link is in german language, can u send me in english version thanks |
5/17/2017 12:49 PM | |
Posts: 27 Rating: (0) |
dear sir can u also send me hsp firmware v4.7 start up file for tiav13. thanks |
5/19/2017 6:22 AM | |
Posts: 27 Rating: (0) |
|
5/19/2017 8:21 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, there is no adress for run,fwd,rev,speed or speed reference in the G120! The G120 dosn't work in this way over profinet! With Profinet the communication between PLC and Drive is implemented with the PROFIDrive Standard. With this you have defined Telegrams with Control and status words and Speed values in the Telegram. To control the drive you use the technology object and the Motion Control Commands and with this the PLC create the telegraminformation and sen it to the drive. The received data are interpreted and used in the drive. You can also use the Drivelib function blocks to control the drive: https://support.industry.siemens.com/cs/ww/en/view/109475044 Regards Christoph P.S. please stop quoting ! only click on answer! |
Last edited by: ChristophD at: 5/19/2017 8:25:57 AM |
|
Follow us on