1/15/2013 9:56 PM | |
Posts: 52 Rating:
|
Hi All, In my project i am using Profinet CPU S7 315-2 PN/DP. The in built MPI/DP port of the CPU nneds to be configured as DP Slave. When i am doing the slav configuration in hardware configuraion, system is throwing following error: "The process image assignment must not be disabled for the output address area (address 800, length 32 bytes) because the CPU you are using does not support this." It looks like address 800 is not covered under process image area & the same needs to be extended. However I cannt extend the Process image area till 800 as in my project i am also using 2 CP 342-5 DP & their addresses are comming in between I need to add 30 Words in Output & 12 Words in Input of the Slave configuration. Please advise. Please find attached Hardware configuration & some of the configuration snapshots AttachmentSiemens Forum.zip (63 Downloads) |
1/23/2013 7:45 AM | |
Joined: 7/3/2010 Last visit: 3/5/2023 Posts: 30 Rating:
|
Dear Anil Can u upload step7 project? Ninad
|
Follow us on