5/18/2007 5:52 PM | |
Joined: 1/7/2006 Last visit: 12/23/2024 Posts: 2705 Rating: (320)
|
Hi, I have made that once with a PN-CPU and the CP 343-1 Lean as device. There is a example on paper that you may find in the next link PROFINET IO - Configuration & Diagnostics but there is not the CP 343-1 Lean as device... Normally you have to program the CP 343-1 Lean as a device what you are putting on the Profinet of the controller, the CP 343-1EX21. Then you have to program on both sides the data you want to communicate and also have to put the blocks (I believe FB11 and FB12) into both CPU's. On the help of that blocks you might find the right parameters. If you can't find it please put your email-address then in a private message and send the hardware you have set up in the project. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
5/21/2007 5:24 PM | |
Posts: 3 Rating: (0) |
Thank for reply Please find the project Profinet IO here with establishes under STEP 7 V5.4 SP1 and see if possible if it contains a fault (Normally I followed the SIEMENS documentation for the configuration) AttachmentIO_System.zip (897 Downloads) |
Last edited by: tunisun at: 21.05.2007 17:55Last edited by: tunisun at: 21.05.2007 17:52 |
|
5/22/2007 11:43 AM | |
Posts: 5822 Rating: (412)
|
Hello, AttachmentIO_System2.zip (904 Downloads) |
Follow us on