4/13/2015 5:13 PM | |
Joined: 8/12/2010 Last visit: 3/19/2025 Posts: 6 Rating:
|
Hi Im having some issues regarding profinet communication between 2 PLC´s, I hope I can get some help from the specialists ;) The communications is between S7 315-PN/DP (where I made the configuration using put and get) and S7 315 2DP + CP343-1. I can ping both plc´s from the network so the cables look good but the stats is always 25 job in progress and then 2. I cant figure whats the problem. I send the program in the attach (FC1 Ethernet).
BestRegards AttachmentPLC.zip (62 Downloads) |
Follow us on