9/1/2015 11:18 AM | |
Posts: 15 Rating: (0) |
Hi, Is possible to program Siwarex U without S7-300? Thanks, Best Regards. |
9/1/2015 3:07 PM | |
Posts: 206 Rating: (22) |
Hello Ricardo,
It is possible to use the Siwarex U with ET200M as remote IO. With that you couple it to any master that is supporting ProfibusDP or Profinet. If you want to use a weighing electronics as “stand alone” without PLC the Siwarex U is not the choice, you should better use a WP231 see http://w3.siemens.com/mcms/sensor-systems/en/weighing-systems/weighing-electronics/plc-based-weighing-modules/Pages/weighing-module-siwarex-wp231.aspx or you even go for the brand new WT231 weighing terminal where you have nice HMI integrated, see http://w3.siemens.com/mcms/sensor-systems/en/weighing-systems/weighing-electronics/plc-based-weighing-modules/Pages/weighing-terminal-siwarex-wt231.aspx .
Regards ABenno |
This contribution was helpful to1 thankful Users |