Industry Online Support
Technical Forum
9/9/2011 3:30 PM | |
Joined: 3/21/2006 Last visit: 2/10/2025 Posts: 10239 Rating:
|
Hello, As I understood you need to take a backup of the panel in order to transfer it into a new TP177B. If this is true use a Prosave How do you backup/restore with a Windows-based panel? and cable selected from What transfer options are available in the various operator panels? Using WinCC Flex is possible to make a backup if Transfer of the current project file from the configuration computer to the operating unit must be performed using the Upload option "Enable backtransfer". Best regards, Hristo MIhalev |
9/12/2011 10:54 AM | |
Posts: 3037 Rating:
|
Hello, You can see the TP177B on the PC/PG interface on the Profibus?Then you can make a backup over Profibus. Best regards Tweety |
Follow us on