5/17/2023 11:14 AM | |
Joined: 4/10/2006 Last visit: 4/14/2025 Posts: 959 Rating:
|
Hi Guys, I converted a perfectly functional project from version 15.1 to 17 of the Tia Portal.. I managed to load the sw into the cpu...the operator panel is still the same a 6AV2 124-0QC02-0AX1... the compilation of the HMI it's ok but when I try to load the sw into the panel itself the error I enclose comes out.... but is it possible to convert a project from TIA 15.1 to TIA 17 and load the same software both in the CPU and in the operator panel? what should be done differently?? Thank you Roby I was able to load the software into the operator panel... I didn't have to select "Fit" But control orders and other things don't work anymore... Yet in the technical data of the HMI it is not written that it cannot be programmed with TIA 17... Is it possible that everything is so complicated??? Attachmenttia 17.pdf (328 Downloads) |
Last edited by: Roby at: 05/17/2023 11:48:48Last edited by: Roby at: 05/17/2023 11:49:42Setting of my PG M6 Siemens |
|
5/17/2023 1:33 PM | |
Joined: 5/30/2022 Last visit: 4/25/2025 Posts: 634 Rating:
|
Hi Roby, Please install the panel images of V17, check this image, install the exact version update that you have installed: Image Downloads for HMI Operator Panels |
If this information really helps, you could use the Rate function. |
|
Follow us on