8/27/2010 7:16 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello I just upgraded my engineering station from PCS7 V7.1 to PCS7 V7.1 + SP1. After the upgrade, when I open my project and compile the same, I get the error msg. : HARDWARE ERROR: FIle not Found ...\s7asrcom\00000001\setparameterassignment.scl Error Msg Attached.herewith. Any idea, what could be the problem ? Thanks Navnag AttachmentError.zip (145 Downloads) |
There is no such thing as the last bug in a program |
|
8/27/2010 7:35 PM | |
Joined: 9/27/2006 Last visit: 9/10/2024 Posts: 12282 Rating: (2683) |
Hello Navnag; Sorry, no I don't have a specific answer to your problem. But users have enquired as to why some charts are lost, or hardware configurations don't seem to upgrade with this migration 9the Search box shows a few threads on the subject). Have you seen this document, on the procedures to upgrade to SP1? http://support.automation.siemens.com/WW/view/en/39980937 Hope it helps, Daniel Chartier |
Last edited by: O_Moderator at: 9/16/2010 2:07 PMlink edited |
|
7/10/2012 11:50 AM | |
Posts: 836 Rating: (100)
|
Hi. Either your project is damaged (also before), or the problem depends on the installation of windows and / or PCS 7 itself. Have you tried the workaround with the new CPUs? If I would find a virus... espacially Stuxnet, I would do following. Wipe the computer completely (using wiping tool, like Deriks Boot and Nuke). Reinstall everything.... Clean the project on another computer, or inside VMware. Cross check against virus. And then, if you are shure your project is clean, unzip it on the computer. Ragarding Stuxnet / IT security read this FAQ: http://support.automation.siemens.com/WW/view/de/43876783 |
Follow us on