7/31/2023 2:25 PM | |
Joined: 5/30/2022 Last visit: 4/16/2025 Posts: 634 Rating:
|
Hi AutoGen_4001544, Since you have changed your IPC, I would recommend checking if the PG/PC interface of the control panel matches the connection made with the PLC. In the following link to the manual, he comments on different reasons: 200100 - Area pointer alarms project ID (Basic Panels, Panels, Comfort Panels, RT Advanced) |
If this information really helps, you could use the Rate function. |
|
This contribution was helpful to
1 thankful Users |
Follow us on