2/3/2014 2:17 PM | |
Joined: 3/14/2012 Last visit: 10/30/2024 Posts: 22 Rating: (0) |
picture below |
2/28/2014 9:29 AM | |
Joined: 10/10/2005 Last visit: 11/27/2024 Posts: 1921 Rating: (136) |
Hello, consider the following requirments: The project which should be migrated, in the same PC should be installed STEP 7 V5.5, WinCC flexible 2008+SP3 and the STEP 7 (TIA Portal) V12. In refer to Windows XP, you need the SP3. See also the informations in the following FAQ: http://support.automation.siemens.com/WW/view/en/62101547 With best regards |
Last edited by: GrasserF at: 2/28/2014 10:22 AMlink edit |
|
Follow us on