3/26/2018 10:58 AM | |
Joined: 3/26/2018 Last visit: 5/19/2023 Posts: 10 Rating: (1) |
Hi everybody, I checked on the internet and siemens forum, and I found the PDF documentation by Prof. Frink, but I still have my issue. I'm trying to load the "printer driver PDF v1.4" on a TP1200 comfort HMI via ProSave v14.0.1.0. The problem is ProSave can't connect to the HMI. If I ping the panel IP address it's ok, but I tried every combination of PN/IE or Ethernet connection, or other kinds of HMI, but the connection never worked. Can anyone help me? Thanx ------------------------------------------------------------------------------------------ |
Last edited by: mbeghelli at: 3/26/2018 11:12:26 AMLast edited by: mbeghelli at: 3/26/2018 11:36:10 AMLast edited by: Jen_Moderator at: 3/26/2018 12:28:25 PMNew subject after splitting |
|
This contribution was helpful to1 thankful Users |
10/23/2020 4:45 PM | |
Joined: 9/27/2012 Last visit: 3/11/2022 Posts: 18 Rating: (5) |
Hello. If you call prosave from TIA it works! |
This contribution was helpful to3 thankful Users |
6/8/2021 11:14 PM | |
Joined: 7/10/2014 Last visit: 1/22/2025 Posts: 7 Rating: (3) |
worked! thanks |
Follow us on