1/5/2023 6:53 AM | |
Joined: 4/28/2009 Last visit: 7/24/2024 Posts: 347 Rating: (42) |
Hello, PTC resistance is not evaluated as analog signal, drive only compare it to 1650 ohm, if it is under this value, temperature is ok and vice versa. There is no corresponding actual meassured motor temperature in any parameter, so you cannot compare it with threshold. In r35 you have only calculated temperature from motor temperature model in this case. See function diagram 8016 in list manual. With regards Martin |
Last edited by: Martin472 at: 01/05/2023 06:56:22 |
|
This contribution was helpful to1 thankful Users |
Follow us on