11/2/2009 12:12 AM | |
Posts: 223 Rating:
|
On the SMC 30 there are connections on the subd connector for a ptc sensor. This implicates that the ptc on the motor is in the same wire as the motor encoder. Won't this cause problems towards emc because the ptc-sensor is situated insed the motor windings. Otherwise is something goes wrong inside the sensor you might get high voltagefrom the motor windingsindirectly on the encoder. Good thing is that the wires are in the shielded cable from the encoder, so no external emc. Is it a good idea to wire the ptc in the motor encoder cable? |
11/5/2009 5:42 PM | |
Posts: 223 Rating:
|
No experiences? |
Follow us on