3/14/2013 9:05 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713)
|
Hello, I believe this thread might be interesting to read: Microstepping using S7 200 Faq: Positioning Wizard for PTO/PWM in STEP 7 Micro/WIN V4.0 And: How do you position a servo drive axis using the S7-200 pulse interface? Regards, Marcjan |
Problem solved? |
|
3/14/2013 11:10 AM | |
Posts: 12 Rating: (0) |
thanks a lot |
This contribution was helpful to1 thankful Users |
3/14/2013 4:21 PM | |
Posts: 12 Rating: (0) |
I still don't understand the PTO wizard and how to use these subroutines. :$ please help me with a sample program:-/ P.s I feel stupid:$ |
8/22/2013 6:47 AM | |
Joined: 11/12/2011 Last visit: 5/15/2024 Posts: 24 Rating: (0) |
Hello, Please find demo program with MAP servo Q0.0. In this you have set how many pulse required for one rotation in your Stepper drive. 1. If you press I0.2 your motor start rotation continous and stop when you give pluse of i0.0 2. If you press I0.3 You motor start only one rotation at velocity of 100.( As i set 20 pulse for one rotation of motor in my drive. Also check hardware. it is also very important for motor rotation. I think this will help to you. AttachmentDemo.zip (107 Downloads) |