3/23/2014 9:49 PM | |
Joined: 4/11/2011 Last visit: 10/7/2024 Posts: 132 Rating: (7) |
S7 1200 onboard PTO output 100 kHz max.
Looked at the picture and not sure anymore...Flow trough internal resistors 1,2 kOhm ...May be it still works if OPC is connected to 0 VDC. If it still not working then solution is signal board SB1222 (200 kHz). Sinking output is possible. See system manual S71200.
You do not need external resistors because there are internal current limiting resistors 100kOhm. I did project with Yaskawas Junma series servo and Siemens S7 1214DC/DC/DC. Yes, there i used external resistors because internal resistors were small. |
Last edited by: kriipc at: 3/23/2014 11:30 PMLast edited by: kriipc at: 3/23/2014 11:10 PMLast edited by: kriipc at: 3/23/2014 11:03 PMI'm just a human. Mistakes are allowed. |
|
This contribution was helpful to1 thankful Users |
12/27/2016 11:44 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by mitek is split to a separate thread with the subject Diagram connection between S7-1200 and Mitsubishi servo drive. Best regards |
Follow us on