5/7/2012 10:39 AM | |||||||||||||
Joined: 4/19/2008 Last visit: 5/21/2024 Posts: 1525 Rating: (159) |
Hello pooneh, With S7-200 You have only 2 Output with 20KHz Pulse Output, The following table shows the maximum pulse output frequency of the S7-200 CPUs with 24 V DC output A0.0 and A0.1:
How do you position a servo drive axis using the S7-200 pulse interface? & With S7-300 you have to see which module you are using, also what type of load. Let me know Which Module you are planing so I will tell you with Type of load. |
||||||||||||
Ammy |
|||||||||||||
5/7/2012 10:46 AM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Also check this: I'm looking for a really high speed digital output card (DO)
Best regards, Hamid Hosseini |
This contribution was helpful to1 thankful Users |
5/8/2012 7:27 AM | |
Posts: 11 Rating: (0) |
Thank you aLL |
This contribution was helpful to1 thankful Users |