9/15/2010 1:50 AM | |
Posts: 16 Rating: (0) |
Hi, I was trying to follow the examples explained in this link: http://www.autoware.com/english/supp...0/sample16.htm But onS5for windows I can not make it work! Are there other way to do thepulsetrain? Thanks, Bruno |
9/15/2010 3:54 AM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046)
|
Hello BLima it works fine for me in S5 for Windows so I'm not too sure what your problem is. Bear in mind though that Q2.4 will only be ON for ONE scan (OB 1 cycle), so you may not see its activation during online monitoring (as stated in the example: "The output A2.4 should be activated for an instant each second"). Attachedis a screendump which has thethe logic and additionally a counter to "count" and verify thenumber of Q2.4 activations. Note too that the example logic in yourlink uses German mnemonics ("SA" for Off delay Timer) wheras mine uses English mnemonics ("SF" for Off delay Timer). I hope this helps |
Last edited by: fritz at: 9/15/2010 4:17 AMCheers |
|
Follow us on