5/28/2014 10:54 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating:
|
Hello, Please have a look at this FAQ. How do you program the "GET" and "PUT" instructions in the user program of the SIMATIC S7-1200 CPU in order to transfer more than 160 bytes of data? Also, Have a look at this Thread. Sample program: S7 communication GET and PUT instructions Hope this helps. |
Last edited by: Amit_86 at: 5/28/2014 10:57 PMVANDE MATARAM..... |
|
5/28/2014 11:42 PM | |
Posts: 2 Rating:
|
Est-ce possible de vous envoyer ce que j'ai réaliser, car je suis chez moi et je n'ai pas les automates sous la main pour les tester. Je n'ai pas fais le programme, j'ai juste etabli la prise des information d'entrée de la cpu2 avec un put et repris ses information avec un get sur la cpu 1 merci Google trad: Is it possible to send you what I do, because I'm home and I have no controllers on hand for testing. I did not do the program, I just established taking input CPU2 information with a put and resumed with a get information on cpu 1 thank you
AttachmentGavray.zip (58 Downloads) |
Follow us on