9/8/2018 3:51 PM | |
Posts: 2 Rating:
|
Hello everyone, We have two CPU models namely IM151-8 PN/DP and 314C-2 PN/DP. In the IM151-8 CPU we program two blocks of GET(FB14) and PUT(FB15) respectively for communication of read/write data transfer between them. In the program the GET block is working fine(Without errors), but the PUT block is returning error bit as 1 and error code as 1. We saw this error description: "Communications problems",in siemens help document. But how can there be communication problems when the NetPro shows OK(Active) status in both the local and partner connections. And moreover, the Get block is able to run successfully without errors and the immediate put block not able to.. Any reasons for this ? Can some expert help us find out where we are going wrong ? Some immediate help is needed. Thanks Akshay ------------------------------------------------------------------------------------------ |
Last edited by: Akshay_Patil at: 9/8/2018 4:07:46 PMLast edited by: Jen_Moderator at: 9/10/2018 12:02:38 PMNew subject after splitting |
|
Follow us on