3/6/2018 12:51 PM | |
Joined: 7/9/2015 Last visit: 3/14/2025 Posts: 4198 Rating:
|
Hi please check the following FAQ: How do you configure an S7 connection for data communication between an S7-200 and an S7-300 or S7-400 on the Industrial Ethernet?Regards, Towome |
|
|
This contribution was helpful to
1 thankful Users |
3/8/2018 7:32 AM | |
Joined: 4/28/2015 Last visit: 2/24/2025 Posts: 10832 Rating:
|
Hello, thnx for info. Again, I'm not familiar with Smart system so hard to recommend something, but CP343-1 Lean support PUT/GET without problems but only as Server, so partner need to be set only as Client. In other case (as I've recommend before) there is also option for open user communication via Ethernet and TCP/IP protocol. If you have other choice, yes, replace existing system with higher, better. You'll have better solution to future. Good luck. Update: also remember this? S7-200 Smart to S7-300 communication |
Last edited by: Duris_I at: 3/8/2018 7:34:31 AMLast edited by: Duris_I at: 3/8/2018 8:41:08 AMWith best regards... |
|
Follow us on