12/3/2015 12:12 PM | |
Posts: 47 Rating:
|
New question. I have a working Put/Get configuration. But I can only put about 210 bytes to the remote CPU. I need to send about 452 bytes into the same datablock. Can I use two instances of the Put FB? If so, how do I program that so that they don't interfere with each other? Is there any other smart way of doing this? Can I loop the Put function somehow? regards, Olav ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/3/2015 4:55:28 PMNew subject after splitting |
|
12/3/2015 12:41 PM | |
Posts: 5225 Rating:
|
Try this official FAQ... |
This contribution was helpful to
2 thankful Users |
Follow us on