5/23/2014 11:36 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (133) |
Hello To 1.) Important is here the synchronization of the project when multiple users are working on the same project at the same time. See in this case the FAQ which was also helpful for me: To 2.) Regarding migration, there are a lot of informations in the internet. See the overview FAQ: To 3.) Regarding trace function I have no experiences with new functions in V13. I can only recommend to see the hole online help informations. With best regards |
This contribution was helpful to1 thankful Users |
5/23/2014 12:06 PM | |
Joined: 1/5/2011 Last visit: 5/13/2024 Posts: 815 Rating: (121) |
Hi Cicero, thanks for your reply. My goal wasn't really to receive manuals or explanations from Siemens, but rather to receive personal experiences with those new features. I know these features exist andare well documented. Sadly enough despite the efforts of siemens the experience of users might differ from the reaction they expected. So how is your personal experience? Is it all as easy as they make believe? Are the functions useful or are they just overloading TiA with as much features as possible to convince customers to upgrade to the latest version? I guess I just need convincing and not just the "how to's and know how's". Thanks anyway, and hopefully you share your experiences. Kind regards, Jens |
Keep it simple and on-topic. |
|