12/14/2009 2:23 AM | |
Joined: 5/28/2008 Last visit: 10/7/2024 Posts: 4515 Rating: (839) |
Yer is correct. I would like to explain something here. As after the CPU make a start up and begin executing OB1, why the CPU is being interrupted to execute othe OBs? Thus because the parameter called "Priority". Each Interrupt OB, have a priority number or index. So, generally, if the trigger condition of the OB happen while the CPU is executing other lower priority OB, it will be interrupted at a break poit and execute the higher priority OB and then return to the lower priority OB at the break point to continue execution and then return to continue OB1. I would like to attach a file here which descripe how the CPUs execute the programs in the different OBs. AttachmentPRO1_12e_OBs [Compatibility Mode].pdf (1207 Downloads) |
Ayman Elotaify |
|
This contribution was helpful to4 thankful Users |
Follow us on