8/31/2016 9:32 AM | |
Posts: 291 Rating: (1) |
Hello Christoph The screenshots are attached,please see them.The lib LMCIpr will use the lib LMCBasic internal. when i compile the LMCBasic for the device D425v4.1 , it is ok, but when i compile the LMCIpr for the D425V4.1 it says: it is not available for the D425 , does the LMCIpr have more requirements? (FOR examole version ....)?? Thank you very much!
Attachmenterror and setting picture.doc (145 Downloads) |
9/1/2016 3:52 AM | |
Posts: 291 Rating: (1) |
Hello ChristopD I use the Device D425 V4.1, in my project ,i want to use 4 libs, LDPV1 ,LMCBasic ,LMIpr, LPrsH, The LDPV1 and LMCBasic is ok when i compiled them, but the LMIpr and LPrsH have many errors , please see the attachment. Thank you ! AttachmentNeu Microsoft Word-Dokument (2).doc (138 Downloads) |
9/1/2016 10:44 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hi, the FW Files can be downloaded here: https://support.industry.siemens.com/cs/ww/en/view/31045047 Regards |
9/2/2016 11:41 AM | |
Posts: 291 Rating: (1) |
Why i cann't download any of them.. |
9/2/2016 11:44 AM | |
Posts: 1529 Rating: (202) |
I can, even without my VPN in China. |
9/2/2016 11:50 AM | |
Posts: 291 Rating: (1) |
OK, i change another network |
9/2/2016 1:04 PM | |
Posts: 291 Rating: (1) |
Hello ChristophD
The library question has solved! Thank you very much! |
Follow us on