3/31/2014 3:56 PM | |
Posts: 25 Rating:
|
can i use simatic manager of step 7 to open step 5 project? consequently, if yes, can i troubleshoot s5 projects on step 7? |
3/31/2014 4:13 PM | |
Posts: 25 Rating:
|
do you have link where i can learn the requirements for troubleshooting s5 projects... like hardware and software.. |
3/31/2014 4:33 PM | |
Joined: 9/27/2006 Last visit: 5/27/2023 Posts: 12022 Rating:
|
Hello Yes Sayer; The S5 manuals and FAQs are different depending on the family of PLCs (i.e, S5-95U, S5-115U...). Please give us the name of the CPU you are trying to troubleshoot,Your CPU will have such a name as CPU 928, or CPU 103... And give us more information on the CPU hardware, such as whether there is an EEPROM slotted in the CPU (part number) and all communictaion or function modules in the PLC rack, along with a basic description of the troubles you are facing (loss of program, diagnostic LEDs that are active, etc...). For example: S5-90U/S5-95U Programmable Controller System Manual S5-115U Programmable Controller S5-135U CPU 928B - Version -3UB21 Look for the information on the main diagnostic tool in Step 5 called the IStack in these manuals. Also look at the link to the S5 manual proposed earlier. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 3/31/2014 6:27 PMLast edited by: dchartier at: 3/31/2014 4:38 PM |
|
This contribution was helpful to
1 thankful Users |
4/10/2014 12:44 PM | |
Joined: 9/1/2005 Last visit: 5/24/2023 Posts: 4099 Rating:
|
follow up question published by YesSayeris split to a seperate thread with the subject Problem with installing the step 5 software. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on