3/26/2020 12:00 PM | |
Joined: 9/9/2014 Last visit: 7/11/2024 Posts: 246 Rating: (40) |
S7-1200 Programmable controller (V4.2, 09/2016, English) Read the manual above Regarding capacity: It all depends on the modules that you will use. For example, the 6ES7 521-1BL10-0AA0 module has a width of 25 mm. Allocate 200 mm for the PLC, the rest for the modules and then 670/25 = 26 modules (something like this) |
Best Regards |
|
Follow us on