Industry Online Support
Technical Forum
12/14/2008 9:54 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
hi, There are radiomodems for Ethernet, then you need a panel that could communicate via Ethernet, the CPU 314 needs a Ethernet card like a CP 343-1 Lean. It might be not fast enough when a direct coupling is there, if not you could work with Sm@rtService, localy on a Panel and on distance with a PC.... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on