3/3/2017 3:58 PM | |
Joined: 11/3/2012 Last visit: 7/23/2024 Posts: 64 Rating:
|
Hello world!!, I have a EMS system in out plant which is having 8 Slave carriers and 1 master system. Communication between the Slave and master is done using the RCOAX wireless communication system. For better understanding please go through the attached PPTx. The issue which i am facing is communication delay in 2 carriers out of 8 while the rest of the carriers is ok. The hardware structure, programs and wireless devices are same in all the carriers. We have check the signal strength of all carriers and found it lies between 60-90%. please tell me the checkpoint which i need to go through. AttachmentCPU_IM.pptx (95 Downloads) |
3/3/2017 5:18 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, Finally, we need to know what mechanism is used to communicate between the CPU315 and the IM151-8. May be the problem is in the way this is written. |
Best regards |
|
3/4/2017 4:46 AM | |
Joined: 11/3/2012 Last visit: 7/23/2024 Posts: 64 Rating:
|
Hello there, Our wireless system has been configured in 5Ghz and channel 36 and also there are near by wireless system also there some are in 2.4 Ghz and some in 5Ghz but channel 36 is not been using anywhere. For your reference i have attached AP and client configuration files. I will look into the system buffer of AP and Client regarding the overlap and will confirm you. AttachmentWireless.zip (81 Downloads) |
Follow us on