1/9/2008 8:46 PM | |
Joined: 1/7/2006 Last visit: 2/16/2023 Posts: 2705 Rating:
|
Hi, The RCOAX is working with all Scalance W equipment. The limit you could find back in the manual and is depending on distance of the Antenna from the RCOAX, used frequency and the bandwith that you need and of course the length... Your last question is not completely clear for me, do you mean the radius for the montage ? Siemens was not Siemens when there was no handbook of this successfull component: SIMATIC NET Manual RCoax RCoax-Leitung 2,4 GHz, ANT792-4DN, RCoax-Leitung 5 GHz, ANT793-4MN, RCoax Zubehör |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on