12/15/2014 8:05 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, This older PLC have a MMC or not? How do you format or reset an MMC (Micro Memory Card) for SIMATIC S7-300 CPUs? After that load hardware config (with new password) and program again. Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to3 thankful Users |
12/15/2014 8:08 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello jagan.k, If you have original project go to Hardware configuration and change the password but you have to reset the MMC and re-download the program to the CPU How do you format or reset an MMC (Micro Memory Card) for SIMATIC S7-300 CPUs? |
6/27/2016 11:30 PM | |
Posts: 2 Rating: (1) |
contact me if you want how you can solve the problem |
Last edited by: Min_Moderator at: 6/29/2016 12:09:42 PMContact data removed |
|
Follow us on