5/20/2016 4:09 PM | |
Joined: 8/8/2014 Last visit: 6/14/2022 Posts: 52 Rating: (3) |
Hi, Pls advise how to read if the CPU (1214C v.2.2) got into Error state on HMI panel ? Thanks |
5/23/2016 6:46 PM | |
Joined: 6/3/2014 Last visit: 9/26/2024 Posts: 660 Rating: (194) |
Hello eam_rts, this FAQ might help you:
Here is another one, but I don't think it works when the PLC doesn't run.
Haven't tested it, but maybe you can try what NKrir did: Use the "LED" block in the PLC to read the status of the error LED of the PLC. Well, I'd say it depends on the kind of error...
https://support.industry.siemens.com/tf/ww/de/posts/meldeindikator/146740/?page=0&pageSize=10 last post --> see screenshot |
Last edited by: H.J. at: 5/23/2016 6:54:16 PM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on