11/29/2020 6:52 AM | |
Posts: 7 Rating:
|
Hello, I have a similar problem when trying to read float parameters from a SINAMICS module in a S7-1200 PLC. For example, for register r55501 I can read in STARTER the value of 9.51V but in PZD I have a completely different value. I don't have any scaling for this parameter. I saw the answer above and tried in S7-1200 to multiply the PZD value with the 0x4000 0000 (value 2 in float) and still it stil wasn't correct. Sorry for the rookie question, but do you have a suggestion how can this operation be applied in my case? Thank you, Oana ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/30/2020 11:13:46New subject after splitting |
|
Follow us on