4/20/2012 11:15 AM | |
Joined: 10/11/2006 Last visit: 6/5/2024 Posts: 5857 Rating: (793)
|
Hello, if you needto send a parameter which is not "connectalbe", you can read it with acyclic communication - see following link: http://support.automation.siemens.com/WW/view/de/58820849 |
With best regards, |
|
4/20/2012 11:52 AM | |
Joined: 5/28/2008 Last visit: 6/9/2024 Posts: 4509 Rating: (837) |
Your telegram selection is correct. Telegram 20. As per attached file, 5th word contains Power reading (output active power). Value is 0 - 4000 Hex = 0 - 16384d. For more info, download the complete manual from this link: Please note that 4000 Hex or 16384 d is equal to value of P 2004 (reference power). Please have a look on parameters as per this manual: From P2000 to P2004 (Refence Parameters). These parameters should be taken into consideration when ever you try to read electric parameters from inverter. Value of these parameters is equavalent to 4000 Hex. Another inportant parameter: P0922 which you have to use when you sellect telegram. In your case you should Put P0922 =20. Hope this helps. P2001
AttachmentOPI_CU240S_25939052_V3_0_en.pdf (420 Downloads) |
Ayman Elotaify |
|
5/7/2012 5:43 PM | |
Joined: 8/9/2011 Last visit: 11/1/2023 Posts: 324 Rating: (19) |
Hellow Ajay Gupta what is free telegram configuration with BICO to connect r39 coz i gone thru the manuals and all but i couldn't find a way out. Is there any s7-1200 sample program regarding this? Thanks |
"Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
5/12/2012 4:57 AM | |
Joined: 8/9/2011 Last visit: 11/1/2023 Posts: 324 Rating: (19) |
Thank you huggy_d1i got it done |
"Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
5/12/2012 5:00 AM |
|
Joined: 8/9/2011 Last visit: 11/1/2023 Posts: 324 Rating: (19) |
Thank you huggy_d1I got it done |
"Any intelligent fool can make things bigger, more complex. It takes a touch of genius -- and a lot of courage -- to move in the opposite direction.":):) |
|
Follow us on