10/18/2015 5:55 PM | |
Posts: 5 Rating:
|
good morning.....i cant read the temp properly from my rtd sm1231 mobule...what i must do... i must put in my programm any converter? my in put is IW68..i use one mobule rtd with 8 inputs and one rtd 4 inputs and i must read 12 temp.. the pt100 is 2 wire sensors..my plc is s7-1200 1214c dc/dc/dc i must read the temp to control 10 valves for one cooling system... this is the one proplem the ather one is one pid control that i must do...from the same plc the two analog in puts in must control one hiting system with two analog output valves 0-10 vdc.. the operetor will set the temp in 4 steps in every step the operetor will set and the temp and the time how much it wil stay at this temp the boiler... difficult?? i have one 6ES7 232-4HD32-0XB0 for analog out i have one 6ES7 231-5PF32-0XB0 for pt 100 i have one 6ES7 231-5PD32-0XB0 for pt100 i have one ktp1000 v12 for control and monitoring i have one 6ES7 223-1BL32-0XB0 for inputs outputs my plc 6ES7 214-1AG31-0XB0 my step is v12 sp1 Thanks you vasilhs... ------------------------------------------------------------------------------------------ |
Last edited by: barotas_greece at: 10/18/2015 6:12:12 PMLast edited by: barotas_greece at: 10/18/2015 6:13:35 PMLast edited by: Min_Moderator at: 10/19/2015 11:15:09 AMNew subject after splitting |
|
10/19/2015 9:37 AM | |
Posts: 5 Rating:
|
thangs for your answer my frend...my input reference the numper 19.888 the temp is 19.8? who i can take this numper? i must convertit? same who? |
10/19/2015 10:44 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
have a look in the system manual of S7-1200 chapter A.9.2.1 page 928 and further: SIMATIC S7 S7-1200 Programmable controllerhope this helps,regards |
FCK WAR! |
|
10/19/2015 10:52 AM | |
Posts: 5 Rating:
|
thangs you again my frend... what to choose for my application? your suggestion? |
10/19/2015 11:22 AM | |
Posts: 5 Rating:
|
no i mean what converter to put in the programm to take the temp from the pt100.. now my input says 19880.. who i can convertit in the temp.. |
Follow us on