Industry Online Support
Technical Forum
6/30/2012 2:01 AM | |
Joined: 11/1/2009 Last visit: 10/30/2022 Posts: 5 Rating:
|
Ekte Siwarex CS modul icin okuma fonksiyonu verilmistir. Ornek konfigrasyonda IM151-8 CPU kullanılmistir. Uygulayacilar, IM151 Interface moduller icinde ornekteki fonksiyonu kullanabilirler. Basari dileklerimizle. --------------------------------------------------------------------------------------------------------------------------------------------------- Given function block for Siwarex CS reading at attachment. IM151-8 CPU using at example configration. Practitioners, Another IM151 Interface modulesuse in the sample function. Best regards. ihsan KAYMAN AttachmentReadin_1.zip (96 Downloads) |
Last edited by: rapido4 at: 6/30/2012 2:10 AM |
|
7/9/2012 11:39 AM | |
Posts: 206 Rating:
|
Hello Rapido, it is possible to use the IM151-8CPU with the example project of Siwarex CS. Please use the last version that you find here: http://support.automation.siemens.com/WW/view/en/25822042 Use the program SICS_CPU and adapr your hardware. Regards ABenno |
Follow us on