Industry Online Support
Technical Forum
7/3/2013 7:00 AM | |
Joined: 4/17/2012 Last visit: 8/13/2022 Posts: 474 Rating:
|
Hi, Here i attached the file for you reference. This is having two PDL file . one if for main picture other one is common motor faceplate. this starter_fvnr is called in other screen. please check it and use the tag prefix based on the project. inside the lp_dosing screen . there is a picture window named as started_fvnr.pdl.this object name is m1_1. there is a text M1_1 window in the name os m1_1. this is act as a button. when ever your press this button pop up will come
AttachmentNew Folder.zip (351 Downloads) |
Follow us on