9/26/2012 12:12 PM | |
Joined: 4/24/2006 Last visit: 1/17/2025 Posts: 8807 Rating: (1173) |
Hello Mannhummel, You can read the System clock of CPU and then make you program. Have a look here: In STEP 7 (TIA Portal) V11, how can you input, read out and edit the date and time for S7-300/400/1200? Which functions are available in STEP 7 V5.5 and in TIA Portal V11 for processing the data types DT and DTL? In STEP 7 (TIA Portal) V11, how can you schedule a program event for an S7-1200? how do you implement a weekly timer for the SIMATIC S7-1200 in STEP 7 V11? Best regards, Wizard |
10/30/2013 11:41 AM | |
Posts: 215 Rating: (6) |
Hello Mannhummel, to program different types of timers DTL-formatted for PLC S7-1200 you also can follow this link: http://support.automation.siemens.com/WW/view/en/78788733 Best regards |
1/5/2015 9:56 AM | |
Posts: 21 Rating: (2) |
This is the tutorial for S7-1200 Realtime functions: https://www.youtube.com/watch?v=jY117f6YryU Hope it can help!
|
Follow us on