6/9/2017 9:05 AM | |
Joined: 12/29/2012 Last visit: 4/2/2025 Posts: 120 Rating:
|
Hi All, I am Using Simotion D410- 2 DP With S7300. I Established The Communication Between S7300 and Simotion Through Profibus. The Machine Was Running Asper the Customer Requirements Untill Last 2 Days. Now The Problem Was The Simotion Goes to STOP Mode SomeTimes. After that They Changed The Simotion Switch Position And Set The RUN Mode Again. I Checked The Diagnostic Buffer But Can't Identify the Root Cause For Stop. So Here i Attached The System Log and Diagnostic Log . Kindly Help Me to Solve this Issue..... AttachmentDiagnostics.zip (305 Downloads) |
Best regards |
|
Follow us on