9/12/2016 2:43 PM | |
Posts: 439 Rating: (108) |
Hello William,
Yes, it is possible to use "SetPLCMode" to bring the PLC from STOP to RUN. (or to "wake him up" →) Long story short, I had to do it for the "Option handling" of the S7-1500/ET200SP I had to do for a customer. The new hardware configuration is enable when you restart the PLC, so this instruction help me create a crazy demo! Configuration Control (option handling) in the central or distributed configuration
I double-check, since I am curious, and Basic panels 2nd and also the 1st generation and Comfort panels are all able to use "SetPLCMode" for an event on a button. For the "Multi panels", it is not possible. So you have a good point, as usual! Have a good day! Hugo |
Last edited by: HugoD at: 9/12/2016 2:55:22 PM |
|
10/9/2020 2:54 PM | |
Posts: 2 Rating: (0) |
What did u find on having to reboot bnr plc on canbus? |
Follow us on