12/7/2015 5:01 AM | |
Posts: 61 Rating:
|
I have a similar application to transfer and receive Data blocks via Profinet between 2x 315-2 DP/PN PLCs I have used the Wizard and example to create the attached application FC6 in both PLCs has the call for SEND and RECEIVE FC6 will be called in OB1 DB42 send to DB402 and DB43 received from DB403 Is someone able to have a look and tell me if it is correct ? ------------------------------------------------------------------------------------------ Attachment113798~1.zip (108 Downloads) |
Last edited by: Min_Moderator at: 12/7/2015 11:14:43 AMNew subject after splitting |
|
Follow us on