Industry Online Support
Technical Forum
7/16/2013 6:48 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011)
|
Hello, 1.) on the _tcpOpenClient function is a paramter serverAdress which specify the IP Address of the communication partner. If you work with the function _tcpOpenServer the communication partner musst establish a connection with the IP Adress of the SIMOTION. 2.) looks like you use the wrong datatypes. The StructRetXreceive only works with the command _Xreceive, and this function is defined fpr PROFIBUS communication. For TCP communication you must use _tcpSend and _tcpReceive. 3.) Simotion can't write any files on a remote PC. So you must use a other program to get the data to a CSV file on you PC. On the Utilities CD is an example for a communication between SIMOTION C240 an PC . On the PC site a little vbsScript is used. Regards Christoph AttachmentD:\FAQ_TCPIP_V1_0_en.pdf (293 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on