4/29/2015 8:47 PM | |
Joined: 1/28/2009 Last visit: 3/8/2025 Posts: 6860 Rating:
|
Answer: It is possible to establish communication between 2 CPUs via PROFIBUS subnet one via CP342-5 and the other through integral DP port.All possible samples can be found in the following link.For your case, try ( 6518937) What master/slave communication options are available on PROFIBUS DP?AttachmentSamples.pdf (86 Downloads) |
Last edited by: hdhosseini at: 4/29/2015 8:51:56 PM// For unlucky users, the pdf version of target FAQ link is also included :-) |
|
This contribution was helpful to
1 thankful Users |
Follow us on