8/16/2012 11:18 AM | |
Posts: 94 Rating:
|
Dear All, I wanted to know that can we have redundant communication between Astand alone PLC and plant DCS..? If yes, please explain... I have attached a simple block diagram to show red. communication on profibus protocol, please check is it correct. Regards, Arunraje. AttachmentRedundant Communication.pdf (114 Downloads) |
8/17/2012 8:12 AM | |
Posts: 94 Rating:
|
Dear Sir, DCS- ABB800x or PCS7 Stand Alone PLC- S7 200 Network- Profibus DP Regards, ArunRaje |
8/17/2012 9:33 AM | |
Joined: 10/7/2005 Last visit: 3/24/2025 Posts: 3042 Rating:
|
Hello Arunraje the simple answer in that is to use a Y-Link and the links below have all the additional info on it: How is the Y link structured? (note the link to the manual in it too) How do you configure a Y link module with an S7-200 CPU as slave and an S7-400H system? How do you operate anY Link on a redundant ABB system? I hope this helps |
Cheers |
|
This contribution was helpful to
2 thankful Users |
Follow us on