3/20/2025 7:37 AM | |
Joined: 5/6/2022 Last visit: 4/16/2025 Posts: 585 Rating:
|
Hi SandroAutomation, In the application example you share, as you can see, there are two ways, through the system IP or through a script that switches the connection between one PLC and another. Through the system IP the configuration is the same as in the application example. Through the script the configuration is also the same but the script changes. Here you can find a post with an example project adapted for WinCC Unified and some tips to create the script that may help you: "TIP: Connecting a SIMATIC HMI Unified with a SIMATIC S7-1500R/H" Even so, I'm going to look to see if I see more information about this script so I can help you. Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
2 thankful Users |
Follow us on