Industry Online Support
Technical Forum
8/30/2013 10:13 AM | |
Posts: 29 Rating: (1) |
Hello, I have tried to config redundant connections between my panel PC and two S7 300 redundant plc'ssuch as in this topic/tf/WW/en/Posts/78650 But i use WinCC v11 SP2 Professional and IPC677C 19" Touch PN/IE. So, when i tried to compile project, i got message that my HMI device doesn't support "ChangeConnection" system function. Are there any solutions for my problem? Thanks in advance Andrey
|
8/30/2013 1:38 PM | |
Posts: 3037 Rating: (192)
|
Hello See these links: /tf/WW/en/Posts/78626 /tf/WW/en/Posts/88134 /tf/WW/en/Posts/89548 |
9/2/2013 2:24 PM | |
Posts: 29 Rating: (1) |
Tweety, i have read all this articles early, but all of them use WinCC v11 Advanced, but i use WinCC v11 Professional. |
9/3/2013 2:54 PM | |
Posts: 1299 Rating: (136) |
Hello, there is no redundancy package for professional at the moment. K!ke |
10/2/2015 11:40 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by Danilo Barbosa is split to a separate thread with the subject Redundant connections with WinCC v13 Prof. Best regards |
Follow us on