9/10/2011 10:40 AM | |
Joined: 12/24/2010 Last visit: 10/3/2024 Posts: 10 Rating:
|
Can I configure the system as mentioned in the attached file? If yes can you provide with the necessary BOM? I want to use single SCADA Station with at least 6 stand alone PLC systems. SCADA to PLC shall communicate on redundant ethernet as shown in the diagram. ifone connection of the PLC fails other shall become active without disturbing communication. Thanks. HRS AttachmentPLC Config3.pdf (323 Downloads) |
9/12/2011 9:12 AM | |
Joined: 12/24/2010 Last visit: 10/3/2024 Posts: 10 Rating:
|
I want two ethernet cards on PC and Each PLC also have two ethernet cards which creats two separate LAN's |
9/13/2011 1:16 PM | |
Joined: 12/24/2010 Last visit: 10/3/2024 Posts: 10 Rating:
|
I am configuring the system as per the attached pdf, with REDCONNECT. is this system is vald and work fruitfully? AttachmentSimatic Config.pdf (270 Downloads) |
9/14/2011 7:03 AM | |
Joined: 12/24/2010 Last visit: 10/3/2024 Posts: 10 Rating:
|
Hello Rated I am planning to use WinCC Thanks |
Follow us on