5/12/2015 4:12 PM | |
Joined: 9/27/2006 Last visit: 3/26/2025 Posts: 12344 Rating:
|
Hello sam; You could start by looking at the following Application Notes, both of the document links have sections on setting up redundant IM 153-2s: Configuration of Redundant I/O Modules in SIMATIC PCS 7 I have taken the liberty of preparing a printout of the setup procedure as an attachment. One important point: you have planned on using active bus modules (and the special rail for these) to build your redundant Et 200M stations, I hope. If not, please look at section 1.3 in the links of the Application note, this is critical. You will find some descriptions and links to part numbers for active bus modules for a redundant IM 153-2 in the following discussion: simatic s7400 H with io modules 400 redundant Hope this helps, Daniel Chartier AttachmentRedundant IM 153-2 setup.pdf (65 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on